Other Parts Discussed in Thread: TM4C123FE6PM, LM339
Hello,
I see from Table 23-28 on page 1338 of the TM4C123FE6PM Datasheet that 3 pins (PB0, PB1 & PE3) "...Require an External Pull-up". I can understand that PB0 and PB1 may be special as they have USB functionality, but what is going on with PE3? Is the external pull-up required when configured as a GP input? How about as a GP output (ala open drain)? I can find no other mention of a specific requirement for this pin in any of the signal tables, etc...
I would appreciate any insight anyone may have to offer. Thank you!
Regards,
Dave