This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to change the TMS570LS3137 EMAC example .hcg file to PGE chip?

Hi,guys:

I've post a question ealier that let me know that the TMS570LS3137PGE can loaded the emac example without any modification, but the zwt and pge chip have differences on the pins(the zwt have many I/O and so on), so will it occurs any exceptions if I use the pge chip while the program is written using the zwt? If any modification is needed, then how to change the .hcg file of the example which using the zwt to the program I need using pge chip?

Regards,

yong