I have a question about SECDED in the TMS570. I'm sure the answer is simple, but I haven't been able to find it.
My understanding is that ECC is separate for RAM and FLASH. I can see how to enable both of these, and see how to enable an interrupt to be generated if a single error is detected. However, I can't what this interrupt maps. I can also see in the status register where you can see if a double error has been detected, but I can't see where an interrupt can be enabled or where it maps to. For double errors, are there interrupts?
Thanks,
David