This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
Quick question, I am trying to run some test on the Tiva C Series TM4C1294 Board with its CAN Bus. Do I need to use a external CAN Transceiver in order to connect to another CAN device? If so, any suggestion which device is more preferable? If not, please tell me where is the on-board transceiver and the corresponding pin.
Thanks
Hello Luxi,
Yes, you would need a CAN Trasnceiver. About a month back we ran a lot of CAN posts, one of which had the CAN Transceiver mentioned. I would suggest SN65HVD231Q
Regards
Amit
Should you be prototyping - CAN xcvrs are available both in 8 pin, soic and 8 pin DIP. Remember to include termination resistors @ each end. (of course you'll need 2 CAN xcvrs - one for each "end.")