If the 16 MHz crystal Y2 is removed from a Launchpad, the same on-board ICDI can no longer connect to the on-board U1 mcu using the standard CCS debug functionality. It actually connected the first couple of times I hit the debug button, but on the third and all following attempts the connection attempt fails (CORTEX_M4_0: Error connecting to the target). Because it fails at connection time instead of program load, I don' t think it is a program issue. Even when I touch a jumper GND-to-pin40 (OSC0) as per Issue 3 on http://e2e.ti.com/support/microcontrollers/tiva_arm/f/908/t/374640.aspx , it still fails to connect.
Is this spelled out in the datasheet for the TM4C1236GHPM somewhere? All I see is that the mcu has an internal PIOSC at 16MHz which should be sufficient for basic operation (not USB) . Why doesn't the JTAG work without the external crystal? Or of course I could be overlooking something.
Can TI staff replicate this? Thanks.