Other Parts Discussed in Thread: HALCOGEN, RM42L432
I just received my Hercules LaunchPad evaluation kit (RM42x) and I started working on the project 0 tutorial (PWM Generation using the Hercules LaunchPad) which can be found here:
http://www.youtube.com/watch?v=WYjLGBr9n3M
When I try to compile the code (Run->Debug) I get the following error message:
Cannot open source file F021.h
I can find this header file and include its location in the path for the compiler but more error messages for even more absent header files appear when I try to compile. It appears that there are numerous header files that are included in this example code that I could not possibly need for this relatively simple program.
What is going on? If Halcogen can't do this right why do I need it at all?
I should mention that I am running CCS 6.0.1 and Halcogen 04.01.00 on a PC running the Windows 8 OS. I should also note the following. One step of the project video tells me to right-click the project in CCS and the go to the properties window and include the header files that were created previously in Halcogen. I was not able to add the header files by simply opening the "Add file path" selecting "Workspace" and then clicking the include dir as done in the video. The OK button was grayed-out and there was a message that said "One of the elements selected isn't a file". So instead I selected all the files in the include dir and then the OK button worked. In the file path window I then see multiple header files with paths that look like this example:
"${workspace_loc:/${ProjName}/include/adc.h}"
Thank you