Hello everybody,
I have a GUI issue in HalCoGen 4.04 (see screenshot). You can see that the elements (eg buttons) in the foreground compared to the elements in the background (eg bus) are moved. Working with the program is more difficult. I use this program in a virtual machine. Perhaps the problem lies with the graphics drivers. The driver is VMware SVGA 3D. How can I fix the problem?
If further information is required, I'll put it in this post.
Thanks for the help!
Best Regards,
Daniel