This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

uDMA for EPI port in TM4C129

Hi all,

I am using TM4C129NCPDT microcontroller and newhaven NHD-2.4-240320CF-CTXI#-F-ND TFT LCD. I have driven LCD with controller's EPI port. Now I want to use EPI port with uDMA. Is there any sample code available for LCD EPI port?

I run two ADCs and one DAC with three SSI port and use one timer in my code. and I use graphic library of microcontroller to drive LCD. Now while loop of GrStringDraw,GrRectDraw,GrImageDraw etc. functions take much time so LCD refresh time increases.

Is this delay problem can be solved by using EPI on uDMA?