Other Parts Discussed in Thread: ENERGIA
Hi all,
I'm having a very specific issue using the TM4C129XL with an embedded Linux system. I have set the board to transmit data on UART0 (Serial.print in energia.) This works fine if the board is powered on or plugged in AFTER the Linux system has booted up. But, if the linux system is powered up with this dev board plugged in, no data is received on ttyACM0 until the dev board is power cycled. I replicated this issue on my laptop as well.
I have tried other UART devices (arduino) and they do not have this issue with the same system and kernel modules. Does anyone have some insight as to what is going on? I need this board to be able to start and function with no user intervention. I could use some a relay to ensure the board powers on after the linux system but would prefer a software fix!
Thanks!