This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I was implementing three 200kHz Buck convertors. Each Buck is phased shifted and runs every 5us and uses a zero latency interrupt from the ADC to run a fixed point 3p3z controller (software optimized). Every 10ms a SWI timer is run to calculated floating point values for soft start. The idle task just flashes a LED and performs TCP/IP and USB communications.
But I found my SWI function was sometimes hitting some of my asserts. When I looked at “ret” it was between 0 and ADC_VALUE_MAX, or it was “NaN”.
if (ret >= 0.0f && ret <= ADC_VALUE_MAX) { //ok } else { assert(ret >= 0.0f && ret <= ADC_VALUE_MAX); //hits this line }
At first I though it was because I was using floats in my HWI Buck function, so I re-wrote it to use integer maths only.
Then I realized I had to mark the HWI Buck function as “__interrupt” for the correct context saving to occur.
I’ve done all of this and still my SWI function was being corrupted so I decided to write a small test program to reproduce this error. This code doesn’t perform the buck or soft start code, but contains the bits of code that seems to cause the error. I made the SWI code run for almost 10ms and changed the HWI to run just one buck every 5us.
My test (context.zip) program uses the following version of compiler, RTOS, XDC
It has two files,
You just need to add a break point to empty.cpp at line 50 and run. This break point should be hit and you can see either you have a NaN or ret is within range.
assert(ret >= 0.0f && ret <= ADC_VALUE_MAX);
If you have a ETM then it should be very easy to see how the SWI is being corrupted, but I don’t have one ;-(
So far my possible thoughts are
; CAUTION!!! Do NOT single step thru the next instruction ; else, the processor won't arrive at pendSV thru the ; exception mechanism. msr basepri, r0 ; causes pendSV to happen nop ; 2 nops required for prefetch nop ; .endasmfunc
I found that by changing bits of my code I can cause the corruption not to be detected. But I think this just hides the corruption, so I really want to know what is going wrong and not to change my test program to get it working (unless it’s a sys/bios patch)
Any help in this matter would be greatly appreciated.
Chris
hi,
I use Sys/Bios to set up the HWI as shown below
Hwi_Params hwiParams; Hwi_Params_init(&hwiParams); hwiParams.priority = 0; //0 = non-handled, non-zero = Sys/Bios handled hwiParams.enableInt = true; Hwi_create(INT_PWM0_0, (Hwi_FuncPtr)HwiPwmFunc, &hwiParams, NULL);
And I set up the SWI (that is being corrupted) as shown below
Clock_Params clockParams; Clock_Params_init(&clockParams); clockParams.period = 10; clockParams.startFlag = true; Clock_create(SwiClockFunc, 10, &clockParams, NULL);
I think Sys/Bios might be using a 1 ms system timer interrupt which interrupts my SWI, and it's somehow not restoring its context when my HWI interrupts it. But I'm only guessing.
The Sys/Bios saves the FPU registers for me, so I don't need lazy interrupts, and Sys/Bios didn't work for me when I turned it on, and I read somewhere it doesn't work with it anyway. I'm not using FPU in my HWI and the core auto saves CPU registers and the HWI code also saves some more CPU registers, so I don't think it's the HWI code.
I think it's an error in the Sys/Bios code.
cheers
Chris
Christopher Hossack said:I think Sys/Bios might be using a 1 ms system timer interrupt which interrupts my SWI, and it's somehow not restoring its context when my HWI interrupts it.
Unless the timer uses floating point that shouldn't matter I don't think. The rest of the context is saved and restored in hardware
There is a possibility That if you are using a pre-compiled library there is a calling convention difference.. Floating point emulation might make use of the registers differently too, in which case the entire sys/bios would have to be compiled to support it.
Might be an unprotected critical section in your code. I'd lean towards a mismatch between the sys/bios library and your compiler settings if it comes precompiled and you're using it that way.
I don't suppose you have trace capabilities?
Robert
hi,
Unless the timer uses floating point that shouldn't matter I don't think. The rest of the context is saved and restored in hardware
I don't think it's a standard register context save problem. As you say R0/1/2/3/12 LR,PC,xPSR are automatically handled for you.
There is a possibility That if you are using a pre-compiled library there is a calling convention difference
I've created the project using CCS, and as far as I know it's using the correct library. eg I haven't been given any option to change the library. And it all works fine, unless I bombard Sys/Bios with my HWI.
Might be an unprotected critical section in your code
I think it's a unprotected section in the Sys/Bios, but I'm hoping TI will have a look since it they know a lot more about it than me.
I don't suppose you have trace capabilities?
No. The cheapest one I found is ULINKpro for £1000, and my dev board EK-TM4C1294XL doesn't have the correct connector either ;-(. With a ETM I could quickly see who's corrupting the SWI.
cheers
Chris
I'm able to report past "trace" success using J-Link via SWO - but operated under the IAR IDE and w/out the (potential) impact of (any) RTOS. (thus - my report is far from poster's plight - yet (may) suggest a pathway)
Note that should budget be an issue - the J-Link may be purchased at (astoundingly) low-cost (EDU version) - which matches the standard - AND you do not even have to "feign" student status. (just don't use for professional development...)
I wonder if you could "limit" the reach & extent of the RTOS - and via repeated test & observation - identify that (offending) portion of the RTOS which (appears) to wreak such damage...
; CAUTION!!! Do NOT single step thru the next instruction ; else, the processor won't arrive at pendSV thru the ; exception mechanism. msr basepri, r0 ; causes pendSV to happen nop ; 2 nops required for prefetch nop ; .endasmfunc
I don't understand the comment in the code you posted. Why would single-stepping that instruction cause a pendSV? I have that line of code in my RTOS and I single step it without causing any weirdness like a pendSV. If you figure this out, please post a followup.
hi,
I'm not sure what this piece of code is doing, but I don't think it's the problem. I was just highlighting the fact that the author didn't want that piece of Sys/Bios code interrupted.
When I look at the Execution graph I can see the system is being interrupted every 1ms by the system tick HWI and 1ms SWI Post.
You can also my SWI running for about 7ms which gets corrupted.
What isn't shown is my zero latency (eg non-handled Sys/Bios interrupt) which is running every 5us. I think my HWI is interrupting the 1ms system tick HWI which is doing something naughty and relies on the fact that it's code doesn't get interrupt, eg something like the code example I posted.
So I think I will look at ti_sysbios_family_arm_lm4_Timer_isrStub__E (#defined to Timer_isrStub) to see what it's doing.
cheers
Chris
Hi,
sorry, but I missed these comments. I've ordered a J-Link, but while I'm waiting it looks like the XDS100 should work with ETB according to the TI web site (Embedded Trace Buffer - "User can connect, setup ETB and collect via a XDS100, XDS200, or XDS560 class JTAG emulators"), but it doesn't ;-(
I've raised this issue (Can not use the Embedded Trace Buffer (ETB) on a TIVA TM4C1294NCPDT with a xds100v2 JTAG)in a hope for an answer.
cheers
Chris
Sorry to only say this after you have ordered a J-Link, but since you are using CCS you won't be able to use the SWO trace facilities since the http://processors.wiki.ti.com/index.php/J-Link_Emulator_Support which was added for CCS 5.2 only supported basic debug functionality.Christopher Hossack said:I've ordered a J-Link
As of CCS 6.1.2 there is no J-Link support for SWO trace, in that when I attempted to enable Statistical Function Profiling with a TM4C1294NCPDT connected with a Segger J-Link set to use SWD communication got a The specified breakpoint type "Trace" does not exist on this target error.
Full J-Link support for CCS is planned for CCS 6.2 - see https://www.segger.com/ti-code-composer-studio.html
Edit: Re-word as not sure which version of CCS is in use.
We note that past suggestions (by two here) mentioned J-Link AND the superior IDE - IAR.
"Sorrow" is (really) not any requirement as J-Link supports multiple ARM MCUs (vast number of vendors) and out-performs those JTAG probes normally used here...
In time - poster will likely (graduate) to the faster, feature laden MCUs which encompass M0, M3, M4 & M7 - all supported by the top selling, J-Link...
I can repeat the failure, using the following:Christopher Hossack said:
- Compiler version TI v5.2.2
- TI-RTOS for TivaC 2.14.4.31
- XDCtools version: 3.31.1.33_core
It has two files,
- Empty.cpp - the idle task and SWI function
- Isr.cpp – stripped down buck code
You just need to add a break point to empty.cpp at line 50 and run. This break point should be hit and you can see either you have a NaN or ret is within range.
i.e. the same TI-RTOS for TivaC and XDCtools versions, but a later compiler version. The reason is that I didn't have Compiler TI v5.2.2 installed and the CCS updates wasn't showing that exact compiler version as available.
I found that the failure still occurred if changed to use the "latest" TI-RTOS for TivaC 2.16.0.8, i.e. the problem hasn't been fixed by any TI-RTOS updates.
Will attempt to determine the reason for the failure.
Note that I don't have any trace available, as are using a Stellaris ICDI to debug.
[I did attempt to use the XDS110 debug-out on a CC2650 Launchpad but while I could enable SWO trace in the CCS 6.1 debugger was unable to actually capture any SWO trace data]
I also noticed that after that break point had been hit, if the target was set running again ended up with a Hard Fault.Christopher Hossack said:You just need to add a break point to empty.cpp at line 50 and run. This break point should be hit and you can see either you have a NaN or ret is within range.
Rather than set the break point on empty.cpp line 50 I enabled a break point on any Error under any ARM Advanced Features:
This triggers a break point on the first line of ti_sysbios_family_arm_m3_Hwi_excHandlerAsm__I, with a Hard Fault due to a "Invalid State Usage Fault". When the Hard Fault occurred the RTOS Object Viewer reported that the Hwi stack had overrun:
I tried increasing the HWI stack size from 768 to 4096 bytes, but the failure symptom changed to a SYS/BIOS assertion failure:
Starting the example System provider is set to SysMin. Halt the target to view any SysMin contents in ROV. ti.sysbios.gates.GateMutex: line 99: assertion failure: A_badContext: bad calling context. See GateMutex API doc for details. xdc.runtime.Error.raise: terminating execution
The stack backtrace is:
context [Code Composer Studio - Device Debugging] Stellaris In-Circuit Debug Interface_0/CORTEX_M4_0 (Suspended) loader_exit() at exit.c:52 0x00007608 abort() at exit.c:117 0x00007612 xdc_runtime_System_abort__E(unsigned char *)() at System.c:100 0x0000874C xdc_runtime_Error_policyDefault__E(struct xdc_runtime_Error_Block *, unsigned short, unsigned char *, int, unsigned int, int, int)() at Error.c:165 0x0000394E xdc_runtime_Error_raiseX__E(struct xdc_runtime_Error_Block *, unsigned short, unsigned char *, int, unsigned int, int, int)() at Error.c:114 0x000086F8 xdc_runtime_Assert_raise__I(unsigned short, unsigned char *, int, unsigned int)() at Assert.c:34 0x000070CC ti_sysbios_gates_GateMutex_enter__E(struct ti_sysbios_gates_GateMutex_Object *)() at GateMutex.c:101 0x00004520 ti_sysbios_BIOS_rtsLock__I() at empty_pem4f.c:2,581 0x000083F6 fputs(unsigned char *, struct <unnamed> *)() at fputs.c:98 0x00003526 _abort_msg(unsigned char *)() at assert.c:67 0x00007F38 GetAdcIvalue(float)() at empty.cpp:52 0x00004DC4 SwiClockFunc(unsigned int)() at empty.cpp:90 0x000073D8 ti_sysbios_knl_Clock_workFunc__E(unsigned int, unsigned int)() at Clock.c:266 0x00002BB2 ti_sysbios_knl_Swi_run__I(struct ti_sysbios_knl_Swi_Object *)() at Swi.c:118 0x000030BC ti_sysbios_knl_Swi_restoreHwi__E(unsigned int)() at Swi.c:404 0x00005A28 ti_sysbios_family_arm_m3_Hwi_doSwiRestore__I(unsigned int)() at Hwi.c:1,467 0x00008D16 ti_sysbios_family_arm_m3_Hwi_dispatch__I() at Hwi_asm.sv7M:182 0x0000415A (ti_sysbios_family_arm_m3_Hwi_dispatch__I does not contain frame information)
The stack backtrace doesn't seem to make sense, since can't see where the GetAdcIvalue can call _abort_msg(). Suspect there is some sort of memory overwrite occurring.
My previous analysis was incorrect. What was happening was that GetAdcIvalue was using assert() to report a failure, where the assert macro called _abort_msg(). It was calling _abort_msg from an interrupt context which caused the ti.sysbios.gates.GateMutex assertion failure, HWI stack overrun and then Hard Fault.Chester Gillon said:The stack backtrace doesn't seem to make sense, since can't see where the GetAdcIvalue can call _abort_msg(). Suspect there is some sort of memory overwrite occurring.
When GetAdcIvalue() was changed to increment a global variable to indicate a failure, then the test continued to run without suffering a Hard Fault. The RTOS Object Viewer then showed that the hwiStackPeak was 520 and hwiStackSize 768. i.e. the HWI stack is no longer overrunning.
More analysis required into the root cause.
hi,
Following your investigation I also upgraded my environment to
and changed the assert to modify a global variable, eg
int ErrCount = 0; uint32_t GetAdcIvalue(float Value) { float ret; ret = Value / m_ScaleI; if (ret >= 0.0f && ret <= ADC_VALUE_MAX) { //ok } else { ErrCount++; //assert(ret >= 0.0f && ret <= ADC_VALUE_MAX); } return (uint32_t)ret; }
The ErrCount++ was still hit, indicating corruption was still occurring. But at least now the assert wont confuse the issue.
Thank you for looking this. I've been bashing my head against a wall for ages and a fresh point of view is always helpful.
I think the problem is with Hwi_asm.sv7M::ti_sysbios_family_arm_m3_Hwi_dispatch__I, which is called by the HWI 1ms tick timer. I need to step through it one asm instruction at a time and see what its doing, but there is a lot there I just understand., eg Why does this function check which stack the IRP is on? Shouldn't the hardware store the IRP or the handler code just push it anyway?
ti_sysbios_family_arm_m3_Hwi_dispatch__I: .asmfunc ; ; get IRP ; If this hwi switched to MSP then IRP is on PSP stack ; else if this is a nested interrupt then IRP is on current MSP stack ; tst lr, #4 ; context on PSP? ite NE mrsne r1, psp ; if yes, then use PSP moveq r1, sp ; else use MSP ldr r0, [r1, #24] ; get IRP (2nd of 8 items to be pushed)
At this level I still have lots to learn ;-)
cheers
Chris
I ported your example to run on a MSP-EXP432P401R using the following tools:Christopher Hossack said:My test (context.zip) program uses the following version of compiler, RTOS, XDC
(Please visit the site to view this file)
- Compiler version TI v5.2.2
- TI-RTOS for TivaC 2.14.4.31
- XDCtools version: 3.31.1.33_core
The reason for porting to another Cortex-M4F device is that the MSP-EXP432P401R has a XDS110 which supports SWO trace. The intention was to be able to re-create the problem, and then use SWO trace to investigate.
However, in this MSP432 example I haven't been able to get the GetAdcIvalue() function to report an invalid value. By using the debugger confirm the following are happening as in your TM4C129 example:
The MSP432 TI-RTOS .cfg file is an exact copy of the TM4C example. The source files have changed to use MSP432 peripherals instead of TM4C129 peripherals.
The MSP432 example is attached pwmled_MSP_EXP432P401R_TI_MSP432P401R.zip
Not really sure what this MSP432 shows, either I haven't recreated the exact Cortex-M4F TI-RTOS conditions which cause to the TM4C129 failure or something else.
The SWO trace can only sample the PC at a minimum of 64 cycles - see section 4.8.5.1 Trace DWT Event Type Configuration of www.ti.com/lit/pdf/slaa674 (that is a MSP432™ Debugging Tools document but should also apply to SWO trace in a TM4C129 device). Therefore, SWO trace won't be able to capture the exact sequence of instructions leading up to a breakpoint.Christopher Hossack said:I haven't used the SWO trace before, but do you think I will be able to see the last 5us/(1/120MHz) eg 600 instructions, that were executed before it hits my break-point?
One other option for SWO trace is Interrupt Profiling which logs entrance into and exit out of an interrupt, which should allow you to see if one interrupt pre-empts another.Christopher Hossack said:Hopefully this will let me see exactly when the 1ms HWI and my 5us HWI interrupts occurred.
I don't have any experience of using ETM trace. CCS supports the XDS560v2 PRO TRACE Receiver & Debug Probe which has ETM support. However, the XDS560v2 PRO TRACE product page doesn't list ETM support for TM4C129 devices (ETM support is listed for Cortex-A and Cortex-R based devices). Suggest you ask about TM4C129 ETM support on the CCS forum.Christopher Hossack said:Using a different approach I was thinking of using my EK-TM4C1294XL, disabling the on-board JTAG and then wire up a 20 pin Cortex Debug+ETM. Which JTAG debugger would you then use to capture a trace of the instructions?
Hi,
1. If your interrupt handler is standard C, you will not have any issues with context switches. The hardware knows what to do. The Cortex-M doesn't need special handling for interrupt code, and doing so may cause interesting behavior. Installing the function into the interrupt table is an exercise for the reader.
I use the Sys/Bios Hwi_create() function as shown below
Hwi_Params_init(&hwiParams); hwiParams.priority = 0; hwiParams.enableInt = true; Hwi_create(INT_PWM0_0, (Hwi_FuncPtr)HwiPwmFunc, &hwiParams, NULL);
This will all get very interesting at the point where the ISR passes data to from TI/RTOS. You need to ensure that any data that passes between the interrupt handler and the rest of the system is passed atomically. Is it possible that your handler is pre-empting TI/RTOS and corrupting data?
I think my 5us HWI is interrupting the Sys/Bios 1ms system tick, but the Sys/Bios ti_sysbios_family_arm_m3_Hwi_dispatch__I is doing something where it doesn't expect to be interrupt and is ending up corrupting the SWI context.
2. You should dump out the priority table from the NVIC and confirm that your Buck function is actually running at a higher priority than the rest of the system. Beware - the NVIC numbers priorities backwards from what you might expect.
I looked at the NVIC and it looks like my HWI is the highest priority. Here's a screen shot from CCS
3. Check your stacks for overflow.
There are no stack overflows when it hits my break point. The original code called an assert which did cause an overflow, but this is after the corruption. I changed the assert to increment a global variable instead and there were no more stack over flows but still the corruption.
4. The code sample above refers to Cortex-M requirements, if I recall correctly. Manipulating BASEPRI requires barriers/stalls/etc.
So what would happen if a higher priority interrupts occurs when manipulating the BASEPRI register?
thank for your help
cheers
Chris
Hi Chester,
I've got my msp432 dev board and rewrote my test program (based largely on you code, that saved me hours, thank you). I now fails as before. Here's the new zip file
I can see the CPU execution graph as before which works fine. But I then tried to enable interrupt profiling and/or core trace (via the tools menu), but my trace windows always contained no data. Is there some other option I need to set to get trace data appearing? Does it work on your board with your project?
cheers
Chris
For SWO trace to work, in the Target Configuration the "JTAG / SWD / cJTAG Mode" for the XDS110 must be set to "SWD mode - Aux COM port is target TDO pin":Christopher Hossack said:. But I then tried to enable interrupt profiling and/or core trace (via the tools menu), but my trace windows always contained no data. Is there some other option I need to set to get trace data appearing?
I imported your project, and after changing the "JTAG / SWD / cJTAG Mode" to "SWD mode - Aux COM port is target TDO pin" was able to get Interrupt Profiling data. The following shows the end of the Raw Trace viewer at the point a breakpoint was hit in the GetAdcIvalue() function on detecting an invalid value:Christopher Hossack said:Does it work on your board with your project?
There are numerous reports of OVERFLOW in the Trace Status, which I think means the interrupt rate is causing some SWO trace samples to be lost. Haven't yet got any more conclusions on the root cause of the problem.
I think the baud rate for the SWO trace output is derived from the CPU clock, optionally divided with a pre-scaler. In which case simply slowing down the CPU clock won't allow more data to be extracted.Christopher Hossack said:I've just started trying to slow down the CPU clock from 120MHz to 1.2MHz (it seems to stop working below this). I was hoping that running the cpu at slower speeds would allow me to extract more data. So far it's not working, but I'll try again on the msp432 board tomorrow.
If the interrupt rate could be slowed down, and the failure symptoms remain the same, that should allow more data to be collected.
Hi,
If you look at the various posts you will find the download links to two projects that contain the whole code. But here's the HWI code you want
#define _xsmmlar(a,c,acc) (((int32_t)(((int64_t)(a)*(c))>>32))+(acc)) inline void CNTRL_3p3zFixedUnified(CNTRL_DataFixedUnified* pCtrl) { int32_t acc =0; acc = _xsmmlar(pCtrl->m_B3, pCtrl->m_E[2], acc); pCtrl->m_E[2] = pCtrl->m_E[1]; acc = _xsmmlar(pCtrl->m_B2, pCtrl->m_E[1],acc); pCtrl->m_E[1] = pCtrl->m_E[0]; acc = _xsmmlar(pCtrl->m_B1, pCtrl->m_E[0],acc); pCtrl->m_E[0] = pCtrl->m_Kerr*((pCtrl->m_Ref - pCtrl->m_FeedBack)); acc = _xsmmlar(pCtrl->m_B0, pCtrl->m_E[0],acc); acc = _xsmmlar(pCtrl->m_A3, pCtrl->m_U[2],acc); pCtrl->m_U[2] = pCtrl->m_U[1]; acc = _xsmmlar(pCtrl->m_A2, pCtrl->m_U[1],acc); pCtrl->m_U[1] = pCtrl->m_U[0]; acc = _xsmmlar(pCtrl->m_A1, pCtrl->m_U[0],acc); pCtrl->m_Out = (uint32_t)acc; } __interrupt void HwiPwmFunc( void ) { Buck.m_Ref = m_AdcVlimit; Buck.m_FeedBack = m_AdcVout; CNTRL_3p3zFixedUnified(&Buck); MAP_Timer_A_clearInterruptFlag(TIMER_A1_BASE); }
I originally was using the intrinsic function _smmlar, but replaced it with a C-macro to eliminate this as a cause of my problem.
cheers
Chris
Christopher Hossack said:If you look at the various posts you will find the download links to two projects that contain the whole code.
I generally don't download. At best that would be frowned upon.
I'll digest this some but what immediately strikes me is the presence of 64 bit arithmetic.
Robert
hi,
so after a quick look I can state the following.
When corruption occurs the set of events do not look very different from a normal cycle.
The corruption only happens after the PENDSV interrupt
WORKS 18.89us 19.99us Entry to Exception TA1_N 0x1B |
corruption 18.86us 19.96us Entry to Exception TA1_N 0x1B |
I then looked at other cycles when PENDSV occurred and it looks like corruption happens when the 1ms Sys/Bios timer (TA0_0 0x18) is interrupted by my HWI (TA1_N 0x1B) between 0.26us and before 0.33us
8.69us Entry to Exception TA0_0 0x18 10.1us Entry to Exception TA1_N 0x1B |
pass |
18.7us Entry to Exception TA0_0 0x18 0.16us Entry to Exception TA1_N 0x1B |
pass |
8.63us Entry to Exception TA0_0 0x18 10.19us Entry to Exception TA1_N 0x1B |
pass |
18.49us Entry to Exception TA0_0 0x18 0.33us Entry to Exception TA1_N 0x1B |
fail |
9.26us Entry to Exception TA0_0 0x18 9.59us Entry to Exception TA1_N 0x1B |
pass |
9.13us Entry to Exception TA0_0 0x18 9.76us Entry to Exception TA1_N 0x1B |
pass |
8.96us Entry to Exception TA0_0 0x18 9.93us Entry to Exception TA1_N 0x1B |
pass |
8.76us Entry to Exception TA0_0 0x18 10.13us Entry to Exception TA1_N 0x1B |
pass |
18.63us Entry to Exception TA0_0 0x18 0.26us Entry to Exception TA1_N 0x1B |
fail |
I also looked at the vector table to double check the interrupts values
Event | Value | Vector offset | Vector value | Priority register |
TA1_N | 0x1B(27) | 0x6c | 0x37b1(HwiPwmFunc) | pri_11=0 |
TA0_0 | 0x18(24) | 0x60 | 0x3075(ti_sysbios_family_arm_m3_Hwi_dispatch__I) | pri_8=7 |
PENDSV | 0x0e(14) | 0x38 | 0x6eb1(ti_sysbios_family_arm_m3_Hwi_pendSV__I) |
So the MSP432 runs at 48MHz (20ns), so around 15 instructions inside ti_sysbios_family_arm_m3_Hwi_dispatch__I I should find some code that does something strange. I'm not sure if 15 is correct and if anybody would like to suggest a better guess then please let me know.
cheers
Chris
hi,
so after a really fresh cup of coffee I looked at the code in ti_sysbios_family_arm_m3_Hwi_dispatch__I, so see whats going on. I haven't programmed in ARM asm for a very long time, so I'm just guessing about this bit.
tst lr, #4 ; context on PSP? ite NE mrsne r1, psp ; if yes, then use PSP moveq r1, sp ; else use MSP ldr r0, [r1, #24] ; get IRP (2nd of 8 items to be pushed) .if __TI_VFP_SUPPORT__ vstmdb {d0-d7}, r1! ; push vfp scratch regs on appropriate stack vmrs r2, fpscr ; push fpscr too str r2, [r1, #-8]! ; (keep even align) tst lr, #4 ; context on PSP? ite NE msrne psp, r1 ; update appropriate SP moveq sp, r1 .endif
It looks to me that this code is doing the following
I think the problem is that after pushing the vfp scratch registers to R1 (eg either PSP or MSP stack) my HWI kicks in. This then pushes its context to the MSP overwriting the vfp scratch registers.
So this code should really adjust the stack value first and then write the vfp scratch registers.
What do you all think?
cheers
Chris
You are right, This is a major hazard. Assuming that the code in question is actually running (are you really using the __TI_VFP_SUPPORT option?) an interrupt that pre-empts in between the register pushes and the update of the stack pointer is going to over-write the just-pushed registers.
The .if block needs to be wrapped in a cpsid i/cpsie i pair.
This is a TI/RTOS bug...
\Looking at the assembler listing shows the compiler has used the Cortex -M4 SMULL instruction, which multiplies two signed 32-bit operands and produces a signed 64-bit result. There are no calls to library/compiler support functions.Robert Adsett said:It struck me Chris since moving to 64 bits invokes library/compiler support for extended precision operation.
hi,
TI has contacted me on another post I raised and confirmed this is a bug.
"We have been able to reproduce the problem & have filed the SYSBIOS-208 bug to fix this in a future release."
It's nice to know I wasn't going crazy. I'm going to award Chester Gillon with the points for this question, because without his help in getting the ETM working with interrupt profiling I wouldn't of been able to track down the fault. And he went the extra mile and porting my test code to the MSP432 and included idiot proof screen shots of what I needed to do. But I would also like to thank everybody else who helped me.
cheers
Chris
PS Chester, can you add one more post copying TI's statement, so when I mark it as answered your post will appear next to the question.