Hi, I'm using SSI3 on EK-TM4C123GXL and noticed a very strange issue. After the line
SSIConfigSetExpClk(SSI3_BASE, CLOCK_RATE, SSI_FRF_MOTO_MODE_3,SSI_MODE_MASTER, 1200000,16);
The pin PB6 is stuck to logical one. And I cannot use it anymore.
During the SPI communication PB6 and PB7 act as SCK and CS along with pins PD0 and PD1! Even more - PORTB is not enabled at all.
Here is the init SPI3 code:
void initSPI3(void) { // attach spi master to SSI3 SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI3); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD); /* * Configure the appropriate pins to be SSI instead of GPIO. The FSS (CS) * signal is directly driven */ GPIOPinConfigure(GPIO_PD0_SSI3CLK); GPIOPinConfigure(GPIO_PD2_SSI3RX); GPIOPinConfigure(GPIO_PD3_SSI3TX); GPIOPinConfigure(GPIO_PD1_SSI3FSS); GPIOPinTypeSSI(GPIO_PORTD_BASE, GPIO_PIN_3| GPIO_PIN_2| GPIO_PIN_0); GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_1); /* * Set the SSI output pins to 4MA drive strength and engage the * pull-up on the receive line. */ GPIOPadConfigSet(GPIO_PORTD_BASE, GPIO_PIN_2, GPIO_STRENGTH_4MA, GPIO_PIN_TYPE_STD_WPU); GPIOPadConfigSet(GPIO_PORTD_BASE, GPIO_PIN_0| GPIO_PIN_3| GPIO_PIN_1, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD); // Configure the SSI3 port for mode 3, 16 bit data SSIConfigSetExpClk(SSI3_BASE, CLOCK_RATE, SSI_FRF_MOTO_MODE_3,SSI_MODE_MASTER, 1200000,16); SSIEnable(SSI3_BASE); }
CPU runs on 50MHz
Any ideas?