In Lockstep mode the outputs of both ARM cores are compared. My question if CPU1 issues an erroneous command with a compare error that CPU2 does not agree with to a peripheral such as GIO, will the command be issued to the peripheral and then 2 cycles later the ESM error will occur or will the ESM error happen before the output is seen?
Thanks!