This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Just received the DK-TM4C129X development board. Followed the Getting Started Guide for the Quickstart Application. As instructed, connected the board to the internet via ethernet, and powered on the board.
Am having some issues with the default qs-weather application. On starting the board, the application loads up, and a "waiting for data" message is displayed, however after a few seconds a "server busy" message is displayed and there is no change after this. Have attached the respective screens.
I have checked the internet connectivity, there is no issue with that. Am not able to identify what the issue is.
Any help would be greatly appreciated.
Thanks & regards
Yash Bhan
Sai
Thank you so much for the reply, I was using TivaWare version 2.0.1, hence the issue. Just downloaded and installed the latest version of TivaWare. Everything is working perfectly now.
Thanks again for the help!!
Regards
Yash Bhan