Part Number: TM4C1294NCPDT
Tool/software: TI-RTOS
Hi,
How do I change the Interrupt priority of my Timer Interrupt. In the datasheet it shows up as interrupt priority is programmable. But How do i do it??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C1294NCPDT
Tool/software: TI-RTOS
Hi,
How do I change the Interrupt priority of my Timer Interrupt. In the datasheet it shows up as interrupt priority is programmable. But How do i do it??
Shyam,
I understood your question. Let me try to clarify a bit more the answer. Consider a system in which there are only TWO INTERRUPTS enabled: a timer and a GPIO (an external switch). Your program is "doing nothing", on the main while() loop.
The ONLY situation in which you would have a possible interrupt priority need is if BOTH the TIMER and the GPIO triggers at THE SAME TIME (or more specifically, within the same 8ns system cycle). In THAT CASE, the interrupt with higher priority would be serviced first.
But that's quite rare, agree?
Now, let's say again that your program was on idle in the main loop, and you push the switch. Your code execution moves to the ISR (Interrupt Service Routine) that you assigned for the GPIO. While the code is inside that function, even if the TIMER triggers, there is no change on the execution flow - it will still finish the function for the GPIO, and only then it will go into the function for TIMER. Priorities WILL NOT change that.
Next case: if your system has 3 interrupts enabled: the GPIO, the TIMER, and let's say a SYSTICK. And as an example, your code is running inside the SYSTICK routine (which will last maybe some 2us...). Now, there is a much bigger chance that both the TIMER AND the SWITCH interrupts happen during such "longer period", agree? In that case, right after the SYSTICK interrupt function finishes, the interrupt priorities will be evaluated, and whichever between TIMER and GPIO had the highest priority will be executed first.
It is technically possible to enable interrupts while inside ISR's - but I WOULD NEVER recommend that - it will make your system crazy to manage.
Again: make your ISR's very short. Just figure out what caused the interrupt, capture some sort of event status, and set some pos-processing flag. Then, inside you main loop, check for that flag, and do the rest of the processing outside the interrupt routine.
Hope it makes more sense. Otherwise, it is time to look at the time slice diagrams used for explaining interrupts...
Bruno