Part Number: EK-TM4C129EXL
Other Parts Discussed in Thread: TIDM-TM4CFLASHSRAM
Hi Everyone,
I'm trying to debug firmware running on an external flash interfaced via EPI. The firmware is fully functional where the LED blinks every 1 seconds. But i want to debug and do a step by step run. If i try to debug like how we normally do , i get the error "Address exceeds the allowed range", which i can understand since the Application base address is pointing to 0x60020000. But if the normal debug method wont work, how can this be achieved ?
This is currently being implemented on TM4C129EXL eval board without RTOS and I'm using TI compiler. Over time I'm finally going to switch to TI-RTOS with GCC compiler.
Thanks in Advance.
- Prajnith