Hello,
Chapter 17 of the TM4C1292 users Manual describes the QSSI.
Several questions:
For 8 bit frames, how does advanced mode (not bi- or quad- ) modes differ from legacy mode? Are 'enhanced modes' per 17.3.4 the same as 'advanced mode'?
Clearly enhanced mode selects Feescale format. Beyond that, paragraph 17.3.4 describes using the FSSHLDFRM bit of the SSICR1 register to configure SSInFss signaling. Does the MODE bit field of sSICR1 have to select a mode other than Legacy to configure SSInFss signaling?
Other than the restriction to 8 bit frames, how else does does Advanced SSI mode differ from legacy mode?
To operate in Advanced SSI mode requires SPO=0 and SHP=0, and Frescale SPI format. Figure 17-5 describes this protocol. But, neither this figure nor any other fully specifies the frame timing. The figure shows an unspecified period in which SSInClk remains low between the LSB of one frame and the MSB of the next. What is the timing for this mode? What document specifies the timing?
Thanks.
m.r.