This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a custom board of TM4C129NCPDT, I programmed MAC address to my custom board then I tried to dump the TCP echo example.
setup: Used TM4C123 as a dummy Launchpad and used its ICDI to program my custom board as posted
Now the code executes till I get following message in console and waits to get IP:
ss in flash
Starting the TCP Echo example
System provider is set to SysMin. Halt the target to view any SysMin contents in ROV.
Service Status: DHCP : Enabled : : 000
Service Status: DHCP : Enabled : Running : 000
but it does not shows any network added and the IP address.
Ethernet jack: RJ-45 : Pulse jack J3011G21DNL with magnetics
Ethernet cable : Cat5e
I'm not getting any IP address,I couldn't figure out what I've missed out in setup for getting IP and I want to know in the tcp echo example where/how the DHCP is enabled?
Thanks.
Hello Charles,
Thanks for your reply!
For non TI- RTOS Ethernet examples, should I try enet_io, enet_lwip, enet_uip examples from Tivaware?
Thanks.
Hi Charles,
Thanks for your reply!
Charles Tsai said:if you run any one of them what do you see? This is just to make sure if your problem is related to Ti-RTOS NDK configuration or your hardware.
Charles Tsai said:Did you run the TCP echo example on a launchPad. If the launchpad is working then your network and the software should be fine.
The TI-RTOS NDK configurations in my case seems perfect...since I get IP address for TM4C129 Launchpad when I run TCP echo example on it. It seems like this is a hardware issue of my custom board . I ran TCP echo on my board, sometimes I get following message in console,
ss in flash
Starting the TCP Echo example
System provider is set to SysMin. Halt the target to view any SysMin contents in ROV.
Service Status: DHCP : Enabled : : 000
Service Status: DHCP : Enabled : Running : 000
Sometime after this message it goes to idle loop in idle.c and sometimes it randomly shows above message in console for while but after that it gives following error message:
I'm not able to pin point where the problem could be? How should I diagnosis this issue?
FYI: I have used TM4C123GXL's ICDI emulator to program TM4C1294NCPDT in CCS.6.1.1
Regards,
Techinspired
Charles Tsai said:Can you check your RBIAS pin? Is it left unconnected or if you have a 4.87KOhm resistor between the RBIAS to the ground.
yes, I have checked my custom board, it has 4.87k ohm resistor connected between RBIAS and ground.
One more question I wanted to ask, what should be the JTAG frequency while dumping the code in my case which uses TM4C123GXL's ICDI emulator to program a custom board of TM4C129NCPDT ?
What other considerations for Ethernet connections ,should I check in?
Thanks.