Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL2-570LC43: FlexRay example on LAUNCHXL2-570LC43

Part Number: LAUNCHXL2-570LC43

Hello

I trying run flexray example on Launchxl2-50lc43. I download flexray example fo tms570ls31 ->FlexRay_Communication_CCSv5. I read that TMS570LS31 has same register for flexray with TMS570LC43. I have problem with writing register SUCC1 in Fr_ControllerInit function. I want write some configuration in SUCC1 register but every time was PBSY flag set to busy and program stop on red marked line. I have no idea where is problem. 

int Fr_ControllerInit(FRAY_ST *Fray_PST)
{
unsigned int error=0;
// write SUCC1 configuration
Fray_PST->SUCC1_UN.SUCC1_UL = 0x0F1FFB00 | CMD_CONFIG;
// Check if POC has accepted last command
if ((Fray_PST->SUCC1_UN.SUCC1_UL & 0xF) == 0x0) return 1;
// Wait for PBSY bit to clear - POC not busy
while ((Fray_PST->SUCC1_UN.SUCC1_UL & 0x00000080) != 0x0);

// unlock CONFIG and enter READY state
Fray_PST->LCK_UN.LCK_ST.clk_B8=0xCE;
Fray_PST->LCK_UN.LCK_ST.clk_B8=0x31;
// write SUCC1 configuration
Fray_PST->SUCC1_UN.SUCC1_ST.cmd_B4=(0xFB00 | CMD_READY);
// Check if POC has accepted last command
if ((Fray_PST->SUCC1_UN.SUCC1_UL & 0xF) == 0x0) error = 1;
// Wait for PBSY bit to clear - POC not busy
while ((Fray_PST->SUCC1_UN.SUCC1_UL & 0x00000080) != 0x0);
return error;
}

  • Hi Jan,

    The Flexray sample clock (SCLK) is 80MHz. The 80MHz is provided by AVCLK2. The second PLL is typically used as source for AVCLK2. Please make sure AVCLK2 is enabled, and the source for AVCLK2 is the 2nd PLL, and 2nd PLL outout is 80MHz.