Hello,
I have an issue with the board which is based on TMS570LS0432 MCU. Hope somebody could help me with it.
Several days ago I accidently loaded SW to MCU which disables LPO (HF + LF) during startup. At the same time code which disables clock monitoring functionality was not available.
As result I'm not able to start debug session anymore. The following error message appears during each try:
CortexR4: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.100.0)
I have tried to "reanimate" the board with different approaches which have been defined at the forum, such as:
1. "Playing" with nPORST during start of the debug session
2. Trying to connect IcePick and DAP separately and swap Flash and RAM
1st approach was unsuccessfully after 2 hours with playing with it.
Also sometimes this approach leads to the following error:
CortexR4: Error connecting to the target: (Error -6305) PRSC module failed to write to a router register. (Emulation package 7.0.100.0)
Typically debug session restart helps.
2nd approach doesn't work at all, I can connect to IcePick, I can connect to DAP, but I'm not able to see neither Flashh nor RAM, only '?' marks.
Also I tried to check nRST with scope, it is permanently "HIGH".
Does anybody know some additional hint which can help me? Resoldering of the MCU is the last one what I would like to hear :(
Thanks in advance for any help!