Part Number: EK-TM4C123GXL
Other Parts Discussed in Thread: BOOSTXL-RS232
Tool/software: Code Composer Studio
Hello i am trying to use following code to update my variables from pc using UART, but using UARTgetc() i get only single character (i.e if i send 13 i will only receive 3), is there anyway i can get the full number.
Other issue is that i am receiving character but i need integers.
#define TM4C123GH6PM
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_gpio.h"
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "driverlib/sysctl.h"
#include "driverlib/rom_map.h"
#include "driverlib/rom.h"
#include "driverlib/pin_map.h"
#include "driverlib/gpio.h"
#include "driverlib/pwm.h"
#include "driverlib/qei.h"
#include "driverlib/flash.h"
#include "driverlib/adc.h"
#include "driverlib/ssi.h"
#include "inc/tm4c123gh6pm.h"
#include "driverlib/timer.h"
#include "driverlib/interrupt.h"
#include "driverlib/uart.h"
#include "uartstdio.h"
char x;
char y;
int main(void) {
SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
UARTFlowControlSet(UART0_BASE, UART_FLOWCONTROL_NONE) ; // Set UART flow control - NONE
IntMasterEnable(); //enable processor interrupts
IntEnable(INT_UART0); //enable the UART interrupt
UARTStdioConfig(0, 115200, 16000000);
while (1) //let interrupt handler do the UART echo function
{
if (UARTCharsAvail(UART0_BASE))
{
y=UARTgetc();
}
}
}