Part Number: TM4C1294KCPDT
Other Parts Discussed in Thread: UCC27714
Connecting REF2033 output hot into VREF of analog comparator PIN0 (c0+ PC6) input seemed to reduce ADC sample noise in GUI scope widgets, also stopped USB0 client from sudden disconnects of PWM0 activity. However WDOG then reset MCU several times after, external VREF via 5k pot (+3v3/18k to AGND) set to 3.2v fewer DOG resets.
The odd part ADC samples DC bus voltage reading several volts higher until PWM0 trigger speed increased from 1ms up to 80us. The shorted VDD MCU 2v LDO regulator pins and all other used pins show NO curve trace stressing.
Also removed +3v3 LDO with hot air, ground pin pad was slightly grey but 3v3 produced roughly same DC ripple (below capture) as EVM LDO regulator.
The end result after MCU resets thus shorted VDD of an MCU being several months of testing on same PCB at DC bus voltages <100v. Failed MCU again removed from PCB (5x), sure enough VDD pins are shorted to GND, past was VBUS pin the culprit. The wonder of having 2oz plating on TQFP 128 pins, same PCB new MCU less a gold plated socket would be much faster!
New MCU installed - should REF2033 being used as analog comparator 3.2v VREF be causing VDD/VDDA mayhem? Did REF2033 output being connected direct to C0+ PC6 play some part of VDD shorting?