Part Number: TIDM-2PHASE-SUBMTR-FW2
Other Parts Discussed in Thread: MSP-ISO
The Two Phase Embedded Metering Firmware Upgrade reference design shows the communication of multiple devices performed over I2C and finally connected to host using a I2C to RS232 converter.
However there is not an explicit I2C signal we can see there ? could you point as which of the MCU signals SDA and SCL are configured as I2C , is this P1.6 & P1.7 configured as I2c and all boards connected together on this I2C bus and then goes to host ?