This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-2PHASE-SUBMTR-FW2: RS232 to I2C Host Commander connections

Part Number: TIDM-2PHASE-SUBMTR-FW2
Other Parts Discussed in Thread: MSP-ISO

The Two Phase Embedded Metering Firmware Upgrade reference design shows the communication of multiple devices performed over I2C and finally connected to host using a I2C to RS232 converter. 

However there is not an explicit I2C signal we can see there ? could you point as which of the MCU signals SDA and SCL are configured as I2C , is this P1.6 & P1.7 configured as I2c and all boards connected together on this I2C bus and then goes to host ?