Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL, EK-TM4C129EXL
Tool/software: Code Composer Studio
In "tivaware_c_series_2_1_4_178" there is text:
"where ENET_MAC_ADDR0 though ENET_MAC_ADDR2"
that could be corrected (by adding "r": "though" -> "through") to:
"where ENET_MAC_ADDR0 through ENET_MAC_ADDR2"
in line 874 of files:
examples/boards/dk-tm4c123g/boot_serial/bl_config.h
examples/boards/dk-tm4c123g/boot_usb/bl_config.h
examples/boards/dk-tm4c129x/boot_emac_flash/bl_config.h
examples/boards/ek-lm4f232/boot_serial/bl_config.h
examples/boards/ek-lm4f232/boot_usb/bl_config.h
examples/boards/ek-tm4c1294xl/boot_emac_flash/bl_config.h
examples/boards/ek-tm4c1294xl/boot_serial/bl_config.h
examples/boards/ek-tm4c129exl/boot_serial/bl_config.h
Best wishes,
Piotr Kasprzyk