This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Rakesh,
The EMAC internal logic is clocked synchronously on the VCLKA4. The MDIO clock is based on a divide-down of the VCL3.
VCLK3 is the peripheral clock divided down from HCLK which is from PLL1 or PLL2
VCLKA4 can be from VCLK or from PLL1 or PLL2.
You can use only PLL1 for this example. PLL2 is the 2nd option for tis example.