Part Number: TMS570LS0714
Other Parts Discussed in Thread: HALCOGEN,
Hello,
We are using the HalCoGen tool and configuring the CAN bit timing in the BTR register. Could you provide any more information on what HalCoGen is optimizing for, particularly regarding the BRP value?
For example, I'd like to understand why is the BRP chosen to be 49 as opposed to 24 in the example below. The configuration with 24 would double the fBrp to 4MHz, and could have the following parameters: tq = 250ns, SYNC_SEG = 1, PROP_SEG = 10, PH_SEG1 = 3, PH_SEG2 = 2. That would have the same Bit Rate, t_propseg, and Sample Point.
One thought is that HalCoGen is forcing PH_SEG1 = PH_SEG2 or PH_SEG2 = PH_SEG1+1 based on 24.3.2.1 'Calculation of the Bit Timing Parameters' in the TMS570LS0714 reference manual. That requirement is fulfilled by setting BRP=49 but not by setting BRP=24. It also seems reasonable to me that it is choosing BRP=49 based on desiring the highest oscillator tolerance between two viable configurations.
Thanks!
Matt