This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want some modifications in enet_weather example, so that i will refresh data after certain time for e.g 60 second, right now it just update once in starting, i want to refresh data from site after 60 second, please suggest me the best way to do that, what changes i need to in existing example.
Please help.
Hi,
If you look at the UpdateUART() function you will see the below snippet of code. See the highlighted in red where the terminal window is only refreshed every CYCLE_DELAY of delay. The CYCLE_DELAY is defined in the enet_weather.h file with a value of 3000000. You can play with this value to adjust the refresh you want. Or you can use the timer to create a 60s timeout so the UART will only update the terminal window when the timer timeout.
//
// Check if we should scroll the cities.
//
if (g_ui32UARTDelay == 0 && g_ui32ShowCities)
{
//
// Clear the terminal. Print the banner and IP place holder.
//
UARTprintf("\033[2J\033[H");
UARTprintf("Ethernet Weather Example\n\n");
UARTprintf("IP: ");
//
// Print the IP address.
//
PrintIPAddress(g_pcIPAddr, ui32IPaddr);
UARTprintf("\n");
UARTprintf("Hit 'ENTER' to exit\n\n");
//
// Print the current city information.
//
UpdateCity(ui32City, true);
//
// 'Updating' banner.
//
UARTprintf("\n__________________________\n\nUpdating:");
if (g_ui32Cycles >= UPDATE_CYCLES)
{
//
// Reset the cities so that they update.
//
for(ui32Idx = 0; ui32Idx < NUM_CITIES; ui32Idx++)
{
ResetCity(ui32Idx);
}
//
// Indicate that we have reset all of the cities.
//
g_ui32Cycles = 0;
}
//
// Reset the delay.
//
g_ui32UARTDelay = CYCLE_DELAY;
Greetings Charles,
Good job - it is wondered "How" the poster missed this. (Might his 'wants' have justified (some) program investigation?)
May we gently "squawk" over the use of the "Overly Precise" test of "UARTDelay?"
if (g_ui32UARTDelay == 0 && g_ui32ShowCities)
It is suspected that "<=" proves a "more forgiving" operator (thus Safer) - while accomplishing the same code objective...
Hi cb1,
The g_ui32UARTDelay is of the unsigned int type. I did a quick experiment. Both == and <= produces identical disassembly code as the compiler will use BNE to make the branch. If I change the g_ui32UARTDelay to a signed integer type then the == will compile the same code while the <= will use BGT. In all cases, there is no penalty on the code size one way or the other.
Hi Charles,
Yes - ok - yet might the 'possibility' of (any) disturbance or disruption cause the (strict) "==" operator to be missed?
Perhaps - even better - the comparison to "<=3":
In our (long) work designing/developing Control Systems - employing such "forgiving" tests - have resulted in more ROBUST Systems! (i.e. the too precise test invites vulnerabilities - and (really) is NOT needed!)