This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I use the HalCoGen Version 04.07.00 with the TI Processor TMS570LC4357. I check the register values generated from HalCoGen and I have a question about the Pinmux module.
The follwing code line is generated by the HalCoGen Tool:
#define PINMUX_ETPWM_TIME_BASE_SYNC_ENABLE(state) \
(pinMuxReg->PINMUX[165] = (pinMuxReg->PINMUX[165] & PINMUX_ETPWM_TIME_BASE_SYNC_MASK) | (PINMUX_ETPWM_TIME_BASE_SYNC_##state))
But I think in the TI Reference Manual (spnu563.pdf, Version May 2014, table 6.3) this should set to PINMMR166.
Table 6.3:
ePWMx TBCLKSYNC Enable --> Register Adress offset 3A8h --> PINMMR166[1]
What is right ?
Best regards
Lars
Hello Lar,
The code generated through HALCoGen is correct.
1. Synchronize all ePWMx modules to SYNCI
SYNCI is from ePWM1SYNI or N2HET1_LOOP_SYNC. The PINMMR[25:24] is to select the sync signal.
2. Synchronize all ePWMx modules to TBCLKSYNC
This TBCLKSYNC is generated by a register bit in the I/O multiplexing module. PINMMR166[1] is the TBCLKSYNC signal. This bit is cleared (0) by default.
PINMMR[166] is configured by calling
etpwmStartTBCLK();
#define PINMUX_ETPWM_TIME_BASE_SYNC_ENABLE(state) \
(pinMuxReg->PINMUX[165] = (pinMuxReg->PINMUX[165] & PINMUX_ETPWM_TIME_BASE_SYNC_MASK) | (PINMUX_ETPWM_TIME_BASE_SYNC_##state))
is for #1