Part Number: TM4C1294NCPDT
Hello TI Community,
I have been hustling to install the USB driver for the Tiva C connected launchpad (TM4C1294) USB serial example (CDC) on Windows 10.
To clear any confusion I don't mean the debugger USB driver, but the actual hardware USB on-chip of the TM4C1294 MCU.
So, this is how MCU appears in the device manager:
I discovered awhile ago that the old drivers that come with the TivaWare aren't up to date, so I downloaded the patch "SW-TM4C-2.1.4.178.PATCH-1.0", but I this is the error message I get when I try to install the new drivers:
Unfortunately previous threads that discussed the issue didn't have a solution for me. Anyone has been exposed with such problem recently?, it might have to do the latest update to Windows 10 way of handling USB devices enumeration.
Thanks.