Part Number: TM4C123GH6PM
Hello everyone,
I'm a fresher of coding TM4C123GH6PM microcontroller. I have some questions like this:
1) I'm working with I2C on this board. The code is fine and there are no errors in it but I'm unable to write and read the data from the slave. I'm using TMS123GH6PM as a master and AT24C04 as a slave. Here is my code. Please check it for me.
2) I want to use I2C to communicate several TM4C123GXL boards. So how Can I find the address of each I2C module in TM4C123GXL board?
Thanks,
Best regards,
#define ADDRESS_DEVICE 0x50 //0x24HC04 (A0, A1 = LOW)
#include "I2C.h"
void Config_I2C(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C1);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA6_I2C1SCL);
GPIOPinConfigure(GPIO_PA7_I2C1SDA);
GPIOPinTypeI2CSCL(GPIO_PORTA_BASE, GPIO_PIN_6);
GPIOPinTypeI2C(GPIO_PORTA_BASE, GPIO_PIN_7);
I2CMasterInitExpClk(I2C1_BASE, SysCtlClockGet(), true);
}
void I2c_Read_Buffer(uint8_t regAddress, uint8_t *pData, uint8_t length)
{
I2CMasterSlaveAddrSet(I2C1_BASE, ADDRESS_DEVICE, false);
I2CMasterDataPut(I2C1_BASE, regAddress);
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_SINGLE_SEND);
while(I2CMasterBusy(I2C1_BASE));
I2CMasterSlaveAddrSet(I2C1_BASE, ADDRESS_DEVICE, true);
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_BURST_RECEIVE_START);
while(I2CMasterBusy(I2C1_BASE));
pData[0]=I2CMasterDataGet(I2C1_BASE);
uint8_t index=1;
for(index=1;index<length-1;index++)
{
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_BURST_RECEIVE_CONT);
while(I2CMasterBusy(I2C1_BASE));
pData[index]=I2CMasterDataGet(I2C1_BASE);
}
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
while(I2CMasterBusy(I2C1_BASE));
pData[index]=I2CMasterDataGet(I2C1_BASE);
}
void I2c_Read_Char(uint8_t regAddress, uint8_t *pData)
{
I2CMasterSlaveAddrSet(I2C1_BASE, ADDRESS_DEVICE, false);
I2CMasterDataPut(I2C1_BASE, regAddress);
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_SINGLE_SEND);
while(I2CMasterBusy(I2C1_BASE));
I2CMasterSlaveAddrSet(I2C1_BASE, ADDRESS_DEVICE, true);
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);
while(I2CMasterBusy(I2C1_BASE));
*pData=I2CMasterDataGet(I2C1_BASE);
}
void I2c_Write_Buffer(uint8_t regAddress, uint8_t *pData, uint8_t length)
{
I2CMasterSlaveAddrSet(I2C1_BASE, ADDRESS_DEVICE, false);
I2CMasterDataPut(I2C1_BASE, regAddress);
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_BURST_SEND_START);
while(I2CMasterBusy(I2C1_BASE));
uint8_t index=0;
for(index=0;index<length-1;index++)
{
I2CMasterDataPut(I2C1_BASE, pData[index]);
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
while(I2CMasterBusy(I2C1_BASE));
}
I2CMasterDataPut(I2C1_BASE, pData[length-1]);
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_BURST_SEND_FINISH);
while(I2CMasterBusy(I2C1_BASE));
}