Part Number: TMS570LC4357
Dear team supporting the Hecules micros,
(Q1) following the code sequence sketched in section 7.7.4 on p. 377 of the TMS570LC4357's technical reference spnu563a to test the SECDED for implcit reads
Thanks!
Stephan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
Dear team supporting the Hecules micros,
(Q1) following the code sequence sketched in section 7.7.4 on p. 377 of the TMS570LC4357's technical reference spnu563a to test the SECDED for implcit reads
Thanks!
Stephan
Hello Stephan,
This method is to test if the l2FMC SECDED works properly.
As the device is coming out of the device reset sequence, the Flash wrapper reads a configuration word from the TI OTP section of bank 0. These are known as Implicit Reads. This is also readable from a bus master at address F008 0140h.
The reset configuration word (RCR_VALUEx) is defined to be of 42 bits. The remaining bits of the 64-bit word are not implemented and read as zeros.
So the sequence to test SECDED logic during implicit reads should be to read 64 bits from 0xF0080140, mask out the upper 22 bits of the higher-order word, and then compare to the RCR_VALUE register contents.
Good morning, QJ,
I'm sorry but the most interesting part of my question has got stuck somewhere after filling the forum's form.
You may wondered already about the incomplete question.
So my question is:
(Q1) Will an ESM 1.6 or 2.19 error arise if a bus master read of the 64 bits at 0xf0080140 leads to a correctable or a not-correctable bit error?
Thank you for your support!
Stephan
Hi Stephan,
ESM 1.6 or ESM 2.19 will be set if an error occurs when performing the implicit read from 0xF0080140.
Dear QJ,
As i read your answer neither an ESM 1.6 nor an ESM 2.19 error will occur when a bus master read of the address 0xF0080140 is executed.
(Q2) If this is true, how can the signalising of bit errors during implicit reads via ESM be tested if ESM erors 1.6 and 2.19 cannot be stimulated?
I challenge the effectiveness of the procedure called in section 7.7.4
as in my understanding this test won't be sufficient to test the underlaying HW comprehensively:
The decision pass/fail is based on a SW-comparison of raw OTP bits and the OTP bits after SECDED.
That means that there are no HW-flags to be evaluated by SW during that procedure - maybe just because there is no HW-comparator.
I appreciate your efforts answering my questions!
Stephan
Hello Stephan,
Sorry for late response. I will do a test for implicit read on LC43x OTP.