Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN, TPIC1021
Tool/software: Code Composer Studio
I have a problem with the LIN_RX_INT flag.
After sending the header to the slave, the data that comes in response is correct - I observe it on the oscilloscope.
Receiving data in a loop works, but I would like to avoid it and receive data using interrupts.
I set up interrupts in Halcogen, then turned them on in the source code. Unfortunately, the LIN_RX_INT flag does not appear.
Additionally, to check if it is a problem with the interrupt or with the appearance of the flag, I tried to control it in a loop. I used the linIsRxReady (LIN_RX_INT) function for this.
On the oscilloscope, I saw that the data had already arrived and it filled the buffer, but the bit in the register didn't change to 1.
I'm using LIN module and TPIC1021 as converter lin_rx lin_tx to LIN bus. SCI/LIN is not used.
Any tips?