Part Number: MSP432P4011
how to configure TimerA to generate an interrupt every 1 second in msp432
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P4011
how to configure TimerA to generate an interrupt every 1 second in msp432
You can refer to this demo code
https://dev.ti.com/tirex/explore/node?node=AGniU3iLu9cS4gl-1UiIIg__z-lQYNj__LATEST
This works like I expected but I get error when I replace Timer32 with Timer_A0. So how do I Configuring TimerA to 128000 (1s) of MCLK in periodic mode ? I will have to change MAP_Timer32_initModule(TIMER32_BASE, TIMER32_PRESCALER_1, TIMER32_32BIT,
TIMER32_PERIODIC_MODE);
Any idea how do I replace these with TimerA?