Part Number: TMS570LC4357
Hello Experts,
The Safety Manual mentions the CAN13 Bit Error Detection which, if I understand correctly, refers to the SECDED of the DCAN-Modul.
According to the Reference Manual single- and double bit errors can generate an interrupt and the error bits are set.
Additionaly the Data Manual list ESM 1.21, 1.22, 1.23, 1.51, 1.73, 1.74, 1.75 and 1.76 beeing set on bit error. However there is no mention of an error getting signaled to the ESM in the Reference Manual.
(Q1) Will the DCAN always signal the ESM that a bit-error has ocurred or is there a way to configure this?
Thank you and best regards,
Max