This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI Support,
I need help with CMPSS.
I am using: LAUNCHXL-F280025C - BOOSTXL-DRV8323RH - Universal Motor control Lab ( so all original from TI)
Basically, I am trying to validate the CMPSS and Overcurrent protection and it is not working.
I am trying to set to trip to 10A, 7 A, 4 A and driving with 10A to force tripping and nothing happens. Can you help me?
Look the settings below.
Thanks,
Orlando
1 - Hal.h
#define MTR1_IU_CMPHP_MUX 1 // CMPSS1-A11
#define MTR1_IU_CMPLP_MUX 1 // CMPSS1-A11
#define MTR1_IV_CMPHP_MUX 4 // CMPSS3-C4
#define MTR1_IV_CMPLP_MUX 4 // CMPSS3-C4
#define MTR1_IW_CMPHP_MUX 3 // CMPSS1-C7
#define MTR1_IW_CMPLP_MUX 3 // CMPSS1-C7
#define MTR1_CMPSS_DACH_VALUE 2700 // 3308 = 14A / 2917 = 10A / 2700 = 7A / 4095 = 23.56A
#define MTR1_CMPSS_DACL_VALUE 1396 // 788 =-14A / 1179 =-10A / 1396 =-7A / 0001 =-23.56A
2 - Hal.c
CMPSS_configFilterHigh(obj->cmpssHandle[cnt], 4, 4, 3);
CMPSS_initFilterHigh(obj->cmpssHandle[cnt]);
CMPSS_configFilterLow(obj->cmpssHandle[cnt], 4, 4, 3); 3
CMPSS_initFilterLow(obj->cmpssHandle[cnt]);
// Set up COMPHYSCTL register
// COMP hysteresis set to 2x typical value
CMPSS_setHysteresis(obj->cmpssHandle[cnt], 1);
#define MTR1_CMPSS_DACH_VALUE 2700 // 3308 = 14A / 2917 = 10A / 2700 = 7A / 4095 = 23.56A
#define MTR1_CMPSS_DACL_VALUE 1396 // 788 =-14A / 1179 =-10A / 1396 =-7A / 0001 =-23.56A
These setting are just for initilization. The DAC value for comparator will be updated by calling HAL_setMtrCMPSSDACValue(obj->halMtrHandle, objSets->dacCMPValH, objSets->dacCMPValL) in runMotor1Control() in motor1_drive.c file.
The dacCMPValH and dacCMPValL is setting in calcMotorOverCurrentThreshold() in motor_common.h(). So the maximum current is set/limited by the obj->overCurrent_A (motorVars_M1.overCurrent_A ).
You can set the right limitation current by changing the definition value in user_mtr1.h. Or online change the value of the motorVars_M1.overCurrent_A in Expressions Window.
#define USER_MOTOR1_OVER_CURRENT_A (7.0f) // A
2 - Hal.c
Don't need to change anything at here in this hal.c file.