Part Number: TMS320F280025C
Dear team:
Due to hardware problems, customers can only program through C2Prog.
After my client added the sincos function to the project, he found that the program could not be programmed with C2Prog, and an error occurred:
Unable to pad and align after processing hex data
There is no problem in programming with C2Prog without calling the sincos function.
The program code is as follows:
#ifndef C28X_FPU_FAST_RTS_H
#define C28X_FPU_FAST_RTS_H
#ifdef __cplusplus
extern "C" {
#endif
//-----------------------------------------------------------------------------
// Standard C28x Data Types
//-----------------------------------------------------------------------------
#ifndef DSP28_DATA_TYPES
#define DSP28_DATA_TYPES
typedef int int16;
typedef long int32;
typedef long long int64;
typedef unsigned int Uint16;
typedef unsigned long Uint32;
typedef unsigned long long Uint64;
typedef float float32;
typedef long double float64;
#endif
//-----------------------------------------------------------------------------
// Function Prototypes
//-----------------------------------------------------------------------------
float32 sqrt(float32 X);
float32 isqrt(float32 X);
//float32 atan2(float32 y, float32 x);
void sincos(float32 radian, float32* PtrSin, float32* PtrCos);
//-----------------------------------------------------------------------------
//
//-----------------------------------------------------------------------------
#ifdef __cplusplus
}
#endif /* extern "C" */
#endif // - end of C28X_FPU_FAST_RTS_H
//===========================================================================
// End of file.
//===========================================================================
cmd:
BOOTROM : origin = 0x003F0000, length = 0x00001402 IQTABLES : origin = 0x003F1402, length = 0x0000166D /* IQ Math Tables in Boot ROM */ FPUTABLES : origin = 0x003F2A70, length = 0x0000081A /* FPU Tables in Boot ROM */ BOOTROM_EXT : origin = 0x003F8000, length = 0x00007FC0 RESET : origin = 0x003FFFC0, length = 0x00000002 FPUmathTables : > FPUTABLES, ALIGN(8)
May I ask what could be the cause?
Best regards