I need source code of TIDA-01292
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Vaibhav,
We have written TIDA-01292 code for DC-AC conversion (when mains is not present) and AC-DC (For Battery charging). We haven’t tuned this for change over, Faults etc. Main purpose of this code was more towards testing the hardware. Please share below information & I will work with you through your TI Sales contact for sharing this code.
Email ID#
Company name:
Project name:
Regards,
Vikas Chola
Hello Vaibhav,
I had discussion with Dhinesh on the same, you can connect with him for the same.
Regards,
Vikas Chola
Thanks Vikas. I got the firmware files from Dhinesh.
But I have below questions -
1. I would like to implement grid syc feature with this design. I can see multiple main.c files. None of them having grid sync or changer over feature implemented.
2. CheckBatteryStatus & CheckTemperature functions are empty?
3. In main.c only InitEPwm2Gpio() called. Where the other GPIO/PWM init happened?
4. I can see TMS320F28060 & TMS320F28027 CPU are more compatible from this firmware. Any recommendation for grid sync feature with low cost TM320F280x family?
If required, I will share the power board schematic with Dhinesh. The power board is proven & working fine with RX24T Renesas CPU with 20ms change over time up to 600W power.
I kept provision for add on controller board. Target is to replace only CPU board with TMS320F280x Family.
Thanks,
Vaibhav
Hello Vaibhav,
This code examples was written for testing of TIDA-01292 so we have worked on basic examples. For other feature like Grid sync, you should refer other ti design like below:
https://www.ti.com/tool/TIDM-SOLARUINV
As I mentioned, customer needs to complete this as we haven’t worked on this as reference solution. This code was more for hardware testing purpose only.
Regards,
Vikas Chola