Part Number: TMS320F28388D
Hi Team,
Our customer is having similar issue.
They are developing an application with the TMS320F28388D controlCARD. They already created a composer GUI. Now there is one problem. Their applications will still run even if the XDS conenection is not stable or lost. Is there a register with a live status bit? Meaning a register on C2000uC which can be checked if his XDS connection via GUI composer is active or not? So in case of an error in the XDS connection they can "stop" the procedure.