This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I cannot debug my code because the code stops at ESTOP line in device.c
My code builds very well.
I'm using the reference code from the folder below;
C:\C2000Ware_4_02_00_00\training\device\f28004x\getting_started\lab_blinkyled_driverlib
How can I resolve the issue? Why does the debug stops at this line?
I showed it as below;
Hi Ryan,
I push debug button and then play. Then the code halted at ESTOP line.
Which part do you require? What do you need?
By the way, code was RAM based and I changed the build option from RAM to FLASH by using setting FLASH active.
Hi,
I added some ss as below. I think it get error at below line;
" GPIO_setAnalogMode(0, GPIO_ANALOG_DISABLED);"
First one is the first stop and other continuous after I pushing the STEP RETURN button.
Hi Gokhan,
I will forward this to a GPIO expert to further assist you.
Best,
Ryan Ma
Hi Gokhan,
You are trying to set pins that are not Analog Mode capable (they don't need to set analog mode):
// // Check the arguments. // ASSERT(((pin >= 224U) && (pin <= 247U)) || (pin == 22) || (pin == 23));
Regards,
Vince