Part Number: TMS320F28386S
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE,
Hi All,
I have a question about rewriting pragram FLASH via USB.
① I have set the Boot PIN setting for the TI C2000 F2836x USB BOOT as shown in the image, is this OK?
② When I build after configuring with Sysconfig, I get the following error.
Is there any way to resolve this?
C28xx_CPU1: Error during Flash Programming. Address 0x00078008, FMSTAT (STATCMD on some devices) 0x00000030
C28xx_CPU1: File Loader: Memory write failed: Unknown error
③ I saw how to use a USB bootloader from a user program.
Is this possible with the F2838x?
Best Regards,
Ito