This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28386S: Plugram FLASH rewriting via USB

Expert 1325 points
Part Number: TMS320F28386S
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE,

Hi All,

I have a question about rewriting pragram FLASH via USB.

① I have set the Boot PIN setting for the TI C2000 F2836x USB BOOT as shown in the image, is this OK?

② When I build after configuring with Sysconfig, I get the following error.
Is there any way to resolve this?

  C28xx_CPU1: Error during Flash Programming. Address 0x00078008, FMSTAT (STATCMD on some devices) 0x00000030

  C28xx_CPU1: File Loader: Memory write failed: Unknown error

③ I saw how to use a USB bootloader from a user program.
Is this possible with the F2838x?

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/758414/ccs-tms320f2837

Best Regards, 

Ito