Other Parts Discussed in Thread: ADS7853
Using a LAUNXL-F280039C, I wish to read data from ADS7853 through SPI but I want it to do it through CLB. I have a clock on SPIA which I can route it to CLB and a chip select on GPIO. My SPIA Use Case is set to CUSTOM and I am using everything except PTE. This is being done by GPIO as mentioned earlier. Due to hardware constraint in the project I wish to read the data through CLB to have minimal use of the CPU core and dump the data so read in a register and later read it from there.
Is this something that is possible to do? Please let me know the configurational changes that need to be done to do this.