Part Number: TMS320F2800157-Q1
Other Parts Discussed in Thread: DRV8301-Q1, DRV8301
Tool/software:
Hello Team,
We have designed a custom board using F2800157QRHBQ1 and DRV8301-Q1 for BLDC motor control. We followed the universal motor control lab document to validate the hardware using all incremental builds. We have modified the parameters for our custom board using the parameter calculation sheet.
We are able to run the motor using our custom board with level 4 build without any issues till 500 Hz (1400 RPM) but we observe OC LED starts blinking above 500 Hz and at around 560-570 Hz motor stops automatically. We don't see any error on the status registers. But the same motor works fine with the DRV8301 Eval kit.
https://www.ti.com/tool/DRV8301-69M-KIT
Motor Parameters: