This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800157-Q1: F2800157-Q1 FMEDA issue

Part Number: TMS320F2800157-Q1

Tool/software:

Hi Experts,

I am asking for my customer here.

Q1.ADCSOCA0 and ADCSOCB0, The FMEDA pin selection includes ADCSOCA0 and ADCSOCB0. Are these external pins on the chip?

Q2.We can't find the custom diagnostics circled below in the safety manual? Could you point it to us? Thanks.

  • Q1.ADCSOCA0 and ADCSOCB0, The FMEDA pin selection includes ADCSOCA0 and ADCSOCB0. Are these external pins on the chip?

    Let me check on these and get back to you.

    Q2.We can't find the custom diagnostics circled below in the safety manual?

    What you show are the subparts of the SYSTEM and XBAR modules in the MCU. Custom diagnostics tab allows customer to specify their own safety mechanism for covering these subparts. To cover SYSTEM and XBAR customer can use the standard safety mechanisms listed in the "Safety Mechanism Tailoring" tab.  

  • Q1.ADCSOCA0 and ADCSOCB0, The FMEDA pin selection includes ADCSOCA0 and ADCSOCB0. Are these external pins on the chip?

    These are the ADC start of conversion signals generated by the EPWM. These are can be used for debug purposes, but my guess is that customer would not use this function.