Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Refer to above thread,
Answer from Yanming: "Yes. You are right. The Id will be closed to the reference value (=0) of the Id. And you don't need to do anything on Vd and Vq which are the output of the Id&Iq PI/PID controllers. The Id is not dependent on the speed and load. "
Question:
The Id reference should be set to zero in this scenario. However, in the FCL, Id/Iq interacts with Vd/Vq, and there are two PI loops involved. If the Id_Feedback remains non-zero for an extended period, then Id_ref is expected to be zero, indicating that the parameters of the Id PI loop need tuning. Is this correct? Do you have any recommended principles for tuning the Id PI loop?