This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DK: Considerations when using software one-shot trip

Part Number: TMS320F28P650DK

Tool/software:

Hi champs,

I am asking this for our customer.

The user wonders if there is any limitation/concern/consideration when using software one-shot trip of EPWM.

That is,

EPWMx.TZFRC.OST

EPWMx.TZCLR.OST

1)

For example, if a PWM period is 1 sec and this PWM is 100% duty on, and the user uses EPWMx.TZFRC.OST and then use to EPWMx.TZCLR.OST to trip it low and then clear alternatively every 1 ms.

Is it possible to have on and off and on and off like that?

2) As long as the user uses EPWMx.TZFRC.OST and then TZFLG.OST=1, it means the one-shot trip is effective until the user uses EPWMx.TZCLR.OST to clear TZFLG.OST. Is our understanding correct?