Tool/software:
Hi
I found my Windows 11 cannot add RS232/USB driver under Device manager/Ports (COM & LPT), see below:
I tried it on F28379 LaunchPad, no problem.
This causes that I can't use FT232 on the LaunchPad to fetch date from the CPU.
I have used this feature before, I don't know when and how this feature had gone. I changed my PC,
I installed a few CCS versions on my PC, I don't know if any of above cause this issue.
Thanks.
Jiakai
Hello Jiakai
Can you send an image of what else shows in your device manager? Please refer to this E2E in case it helps your case: https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/370982/usb-not-recognized-by-windows-device-manager
Best Regards,
Allison
Hello,
Please also double check with the trouble shooting guide to ensure you are able to connect: https://software-dl.ti.com/ccs/esd/documents/ccsv7_debugging_jtag_connectivity_issues.html#troubleshooting-the-connect-phase
Best Regards,
Allison
Hi Jiakai,
Can you make sure the switch enabling the UART-to-USB bridge on the LaunchPAD is in the correct position for the GPIOs you have selected:
Also, just to verify, you are able to connect the debugger to the LaunchPAD in CCS without issues? And the power LEDs on the board are on when you plug it into your PC?
Best Regards,
Delaney
Hi Delaney,
I have double checked it (JP7: ON, JP6: OFF). I can run code in my LaunchPad without any problem. Power LED is on.
Hello,
Can you please open CCS, open the device .ccxml file and click the "Test connection" button to test your debug connection to the device and ensure there are no issues there?
Best Regards,
Allison
Hi Allison, the followings are the content I got when I hit "Test Connection button:
[Start: Texas Instruments XDS100v2 USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\jye\AppData\Local\TEXASI~1\CCS\
ccs1281\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100/110/510 class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'Sep 26 2024'.
The library build time was '10:09:41'.
The library package version is '20.0.0.3178'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '4' (0x00000004).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the FTDI FT2232 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for FTDI FT2232 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[The log-file for the JTAG TCLK output generated from the PLL]----------
There is no hardware for programming the JTAG TCLK frequency.
-----[Measure the source and frequency of the final JTAG TCLKR input]--------
There is no hardware for measuring the JTAG TCLK frequency.
-----[Perform the standard path-length test on the JTAG IR and DR]-----------
This path-length test uses blocks of 64 32-bit words.
The test for the JTAG IR instruction path-length succeeded.
The JTAG IR instruction path-length is 38 bits.
The test for the JTAG DR bypass path-length succeeded.
The JTAG DR bypass path-length is 1 bits.
-----[Perform the Integrity scan-test on the JTAG IR]------------------------
This test will use blocks of 64 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG IR Integrity scan-test has succeeded.
-----[Perform the Integrity scan-test on the JTAG DR]------------------------
This test will use blocks of 64 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG DR Integrity scan-test has succeeded.
[End: Texas Instruments XDS100v2 USB Debug Probe_0]
Hello,
Thank you for checking - this confirms your JTAG connection, and if your jumpers are correct then the serial connection should be enabled hardware wise. I'll double check with CCS team on any input there but in the meantime have you perhaps tried a different USB cable or board?
Best Regards,
Allison
Hi Allison,
I have changed the other USB cable, and I have used the same USB cable for other LaunchPads and I could communicate to these LaunchPads with USB/RS232.
Jiakai
Hello,
Is this the LaunchPad that you are using?
https://www.ti.com/tool/LAUNCHXL-F28069M
You also mentioned Windows 11. Did you try this with an older Windows version with success?
Thanks
ki
Hi Ki,
I have used F28069M LaunchPad in windows 10 and 11 before, I can use SCI without any problem, but in last month, I have installed a few CCS versions (ccs v11 and ccs v12) and CCS v20/CCS Theia v1.5.1, then I can't use SCI again (but my F28379 LuanchPad SCI works fine).
I don't know if it is because I installed ccs v12 and v20, and caused the conflict.
Thanks,
Jiakai
I tried it on F28379 LaunchPad, no problem.
I see this for my F28069M LaunchPad on both Windows 10 and Windows 11. So I don't think this is a Windows 11 specific issue.
I don't know if it is because I installed ccs v12 and v20, and caused the conflict.
This should not be an issue. My laptop has many many different CCS versions installed and I don't see the issue.
I wonder if the issue is with some hardware problem with the LaunchPad. Can you try it on some other PC and see if you have the same issue?
Thanks
ki
Hi Ki,
I have tested it on another PC, same as before. that is No USB serial Port added for F28069M LaunchPad.
This issue was reported by our customer, our support team confirmed it. I think it is a common issue.
Do I need to upgrade F28069M LaunchPad firmware?
Thanks,
Jiakai
but in last month, I have installed a few CCS versions (ccs v11 and ccs v12) and CCS v20/CCS Theia v1.5.1, then I can't use SCI again
This is on just WIndows 11? Or you see the issue also on Windows 10?
Check this related post:
Note that the referenced wiki page is no longer active. A PDF archive can be found om:
https://software-dl.ti.com/ccs/esd/documents/xdsdebugprobes/files/XDS100.pdf
See page 9 for the FAQ in question.