This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi all
I have experimental board of 28335
and while loading prog into chip following error occurs and program fails
and also i found that chip is getting hot within 30-40 sec when connected to power from usb.
It appears that the target is being held in reset. This may be
due to Wait-In-Reset (WIR) configuration set by the EMU0=0
and EMU1=1 pin settings. If this is the case, DISCONNECT
all CONNECTED devices including icepick and then select
RETRY to clear the WIR configuration.
please help me to solve this prob
i am unable to find problem whether target or emulator is damaged or any thing else.
Nikhil,
Please answer the following questions:
Regards,
Manoj
thanks manoj
i am using TMS320F28335 Experimenter Kit and powered via USB
JTAG Scan chain test passing sucessfully
i tried with another docking station but same error occur.