This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

f28235 Erase operation in progress... and nothing ...

Other Parts Discussed in Thread: CCSTUDIO, TMS320F28235

Dear all, I have developed a firmware application for my TMS320F28235 with and customs board. The application spra958h(David M. Alter) works well in debug mode (RAM project) then I want to program(FLASH project) the flash on-chip memory. I have: 1) CCS3.3 + SR12_CCS_v3.3_SR_3.3.82.13+DCSP_4.30, Flash2833x_API_V210 2) emulator SAU510USB 3) Customs board with TMS320F28235, 30Mhz quarz+18pF cap, JTAG header, boot jumper and etc I do 1) Run On-Chip Flash Programmer 2) Programmer Settings DSP device - f28235 Flash API Interface COFF (.out ) file - C:\CCStudio_v3.3\plugins\Flash28xx\Algorithms\28235\FlashAPIInterface28235V2_10.out Clock Configuration OSCCLK - 30Mhz CLKINDIV - 2 PLLCR - 10 SYSCLKOUT - 150 Mhz I have Device reset detected. Updating locked or unlocked state of target in Flash Programmer. The device is unlocked. **** Begin Depletion Recovery Operation. *** Depletion Recovery Operation succeeded **** End Depletion Recovery Operation. *** **** Begin Frequency Test Operation. *** Frequency Test Operation in progress... Frequency Test Operation succeeded **** End Frequency Test Operation. ***-------- I see 10Khz on gpio00!!! Erase Only Operation in progress... Erase operation in progress.. And nothing happen I`m wait ~5 min, press HALT Disassembler window ................................ ->3FF3E6 761F0180 MOVW DP,#0x0180 3FF3E8 060C MOVL ACC,@12 3FF3E9 ECFD SBF -3,EQ ................................ Which would be the problem? Can anyone help me? Thank you in advance, best regards Vlad