This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear sir,
I have developed the evaluation board for TMS320F2812. i couldnt able to detect the board. how can i debug it. any one can help me.
The spec is:
20MHz, SCI programming using CODE SKIN C2000 prgorammer.
All Voltages are fine.
thanks in advance.
Malaiyappan
How do you have the GPIOs configured which are used to determine the boot mode?
To boot from SCI_A the following is required:
GPIOF4 = 0
GPIOF12 = 0
GPIOF3 = 1
GPIOF2 = 1
Secondly, are you able to interact with the target hardware using Hyperterminal as suggested in Section 3.3.3 of the SPRAAQ2?